The Apache Tomcat Servlet/JSP Container

Apache Tomcat 7

Version 7.0.81, Aug 11 2017
Apache Logo

Links

User Guide

Reference

Apache Tomcat Development

Connectors How To

Table of Contents
Introduction

Choosing a connector to use with Tomcat can be difficult. This page will list the connectors which are supported with this Tomcat release, and will hopefully help you make the right choice according to your needs.

HTTP

The HTTP connector is setup by default with Tomcat, and is ready to use. This connector features the lowest latency and best overall performance.

For clustering, a HTTP load balancer with support for web sessions stickiness must be installed to direct the traffic to the Tomcat servers. Tomcat supports mod_proxy (on Apache HTTP Server 2.x, and included by default in Apache HTTP Server 2.2) as the load balancer. It should be noted that the performance of HTTP proxying is usually lower than the performance of AJP, so AJP clustering is often preferable.

AJP

When using a single server, the performance when using a native webserver in front of the Tomcat instance is most of the time significantly worse than a standalone Tomcat with its default HTTP connector, even if a large part of the web application is made of static files. If integration with the native webserver is needed for any reason, an AJP connector will provide faster performance than proxied HTTP. AJP clustering is the most efficient from the Tomcat perspective. It is otherwise functionally equivalent to HTTP clustering.

The native connectors supported with this Tomcat release are:

  • JK 1.2.x with any of the supported servers
  • mod_proxy on Apache HTTP Server 2.x (included by default in Apache HTTP Server 2.2), with AJP enabled

Other native connectors supporting AJP may work, but are no longer supported.

Comments

Notice: This comments section collects your suggestions on improving documentation for Apache Tomcat.

If you have trouble and need help, read Find Help page and ask your question on the tomcat-users mailing list. Do not ask such questions here. This is not a Q&A section.

The Apache Comments System is explained here. Comments may be removed by our moderators if they are either implemented or considered invalid/off-topic.


Copyright © 1999-2017, Apache Software Foundation