The Apache Tomcat Servlet/JSP Container

Apache Tomcat 7

Version 7.0.81, Aug 11 2017
Apache Logo

Links

User Guide

Reference

Apache Tomcat Development

Load Balancer HOW-TO

Table of Contents
Using the JK 1.2.x native connector
Please refer to the JK 1.2.x documentation.
Using Apache HTTP Server 2.x with mod_proxy
Please refer to the mod_proxy documentation for Apache HTTP Server 2.2. This supports either HTTP or AJP load balancing. This new version of mod_proxy is also usable with Apache HTTP Server 2.0, but mod_proxy will have to be compiled separately using the code from Apache HTTP Server 2.2.
Comments

Notice: This comments section collects your suggestions on improving documentation for Apache Tomcat.

If you have trouble and need help, read Find Help page and ask your question on the tomcat-users mailing list. Do not ask such questions here. This is not a Q&A section.

The Apache Comments System is explained here. Comments may be removed by our moderators if they are either implemented or considered invalid/off-topic.


Copyright © 1999-2017, Apache Software Foundation