The Apache Tomcat Servlet/JSP Container

Apache Tomcat 7

Version 7.0.81, Aug 11 2017
Apache Logo

Links

Top Level Elements

Executors

Connectors

Containers

Nested Components

Cluster Elements

web.xml

Other

The Service Component

Table of Contents
Introduction

A Service element represents the combination of one or more Connector components that share a single Engine component for processing incoming requests. One or more Service elements may be nested inside a Server element.

Attributes
Common Attributes

All implementations of Service support the following attributes:

AttributeDescription
className

Java class name of the implementation to use. This class must implement the org.apache.catalina.Service interface. If no class name is specified, the standard implementation will be used.

name

The display name of this Service, which will be included in log messages if you utilize standard Catalina components. The name of each Service that is associated with a particular Server must be unique.

Standard Implementation

The standard implementation of Service is org.apache.catalina.core.StandardService. It supports the following additional attributes (in addition to the common attributes listed above):

AttributeDescription
Nested Components

The only components that may be nested inside a Service element are one or more Connector elements, followed by exactly one Engine element.

Special Features

There are no special features associated with a Service.

Comments

Notice: This comments section collects your suggestions on improving documentation for Apache Tomcat.

If you have trouble and need help, read Find Help page and ask your question on the tomcat-users mailing list. Do not ask such questions here. This is not a Q&A section.

The Apache Comments System is explained here. Comments may be removed by our moderators if they are either implemented or considered invalid/off-topic.


Copyright © 1999-2017, Apache Software Foundation