The Apache Tomcat Servlet/JSP Container

Apache Tomcat 7

Version 7.0.81, Aug 11 2017
Apache Logo

Links

Top Level Elements

Executors

Connectors

Containers

Nested Components

Cluster Elements

web.xml

Other

The Jar Scanner Component

Table of Contents
Introduction

The Jar Scanner element represents the component that is used to scan the web application for JAR files. It is typically used during web application start to identify configuration files such as TLDs or web-fragment.xml files that must be processed as part of the web application initialisation.

A Jar Scanner element MAY be nested inside a Context component. If it is not included, a default Jar Scanner configuration will be created automatically, which is sufficient for most requirements.

Attributes
Common Attributes

All implementations of Jar Scanner support the following attributes:

AttributeDescription
className

Java class name of the implementation to use. This class must implement the org.apache.tomcat.JarScanner interface. If not specified, the standard value (defined below) will be used.

Standard Implementation

The standard implementation of Jar Scanner is org.apache.tomcat.util.scan.StandardJarScanner. Additional attributes that it supports (in addition to the common attributes listed above) are listed in the table.

There are several system properties that control what JAR files are skipped by JarScanner. Those properties are lists of file name pattern. The patterns are separated by comma (','). The leading and trailing whitespace characters in a pattern are ignored. The patterns are matched case-sensitively. The following two special characters are supported:

  • '*' — means zero or more characters,
  • '?' — means one and only one character.
AttributeDescription
scanAllDirectories

If true, any directories found on the classpath will be checked to see if they are expanded JAR files. The default is false.

Tomcat determines if a directory is an expanded JAR file by looking for a META-INF sub-directory. Only if the META-INF sub-directory exists, the directory is assumed to be an expanded JAR file.

scanAllFiles

If true, any files found on the classpath will be checked to see if they are Jar files rather than relying on the file extension being .jar. The default is false.

scanClassPath

If true, the full web application classpath, including the shared and common classloaders and the system classpath (but not the bootstrap classpath) will be scanned for Jar files in addition to the web application. The default is true.

scanBootstrapClassPath

If scanClassPath is true and this is true the bootstrap classpath will also be scanned for Jar files. The default is false.

Nested Components

No components may be nested inside a Jar Scanner element.

Special Features

No special features are associated with a Jar Scanner element.

Comments

Notice: This comments section collects your suggestions on improving documentation for Apache Tomcat.

If you have trouble and need help, read Find Help page and ask your question on the tomcat-users mailing list. Do not ask such questions here. This is not a Q&A section.

The Apache Comments System is explained here. Comments may be removed by our moderators if they are either implemented or considered invalid/off-topic.

Comments are disabled for this page at the moment.

Copyright © 1999-2017, Apache Software Foundation