| Links User Guide Reference Apache Tomcat Development | The Tomcat JDBC Connection Pool| Introduction |  | 
  The JDBC Connection Pool org.apache.tomcat.jdbc.poolis a replacement or an alternative to the Apache Commons DBCP
  connection pool. So why do we need a new connection pool? Here are a few of the reasons: 
      Commons DBCP 1.x is single threaded. In order to be thread safe
          Commons locks the entire pool for short periods during both object
          allocation and object return. Note that this does not apply to
          Commons DBCP 2.x.Commons DBCP 1.x can be slow. As the number of logical CPUs grows and
          the number of concurrent threads attempting to borrow or return
          objects increases, the performance suffers. For highly concurrent
          systems the impact can be significant. Note that this does not apply
          to Commons DBCP 2.x.Commons DBCP is over 60 classes. tomcat-jdbc-pool core is 8 classes,
          hence modifications for future requirement will require much less
          changes. This is all you need to run the connection pool itself, the
          rest is gravy.Commons DBCP uses static interfaces. This means you have to use the
          right version for a given JRE version or you may see
          NoSuchMethodExceptionexceptions.It's not worth rewriting over 60 classes, when a connection pool can
          be accomplished with a much simpler implementation.Tomcat jdbc pool implements the ability retrieve a connection
          asynchronously, without adding additional threads to the library
          itself.Tomcat jdbc pool is a Tomcat module, it depends on Tomcat JULI, a
          simplified logging framework used in Tomcat.Retrieve the underlying connection using the
          javax.sql.PooledConnectioninterface.Starvation proof. If a pool is empty, and threads are waiting for a
          connection, when a connection is returned, the pool will awake the
          correct thread waiting. Most pools will simply starve. Features added over other connection pool implementations 
      Support for highly concurrent environments and multi core/cpu systems.Dynamic implementation of interface, will support java.sqlandjavax.sqlinterfaces for
          your runtime environment (as long as your JDBC driver does the same), even when compiled with a lower version of the JDK.Validation intervals - we don't have to validate every single time we use the connection, we can do this
          when we borrow or return the connection, just not more frequent than an interval we can configure.Run-Once query, a configurable query that will be run only once, when the connection to the database is established.
          Very useful to setup session settings, that you want to exist during the entire time the connection is established.Ability to configure custom interceptors.
          This allows you to write custom interceptors to enhance the functionality. You can use interceptors to gather query stats,
          cache session states, reconnect the connection upon failures, retry queries, cache query results, and so on.
          Your options are endless and the interceptors are dynamic, not tied to a JDK version of a
          java.sql/javax.sqlinterface.High performance - we will show some differences in performance later onExtremely simple, due to the very simplified implementation, the line count and source file count are very low, compare with c3p0
          that has over 200 source files(last time we checked), Tomcat jdbc has a core of 8 files, the connection pool itself is about half
          that. As bugs may occur, they will be faster to track down, and easier to fix. Complexity reduction has been a focus from inception.Asynchronous connection retrieval - you can queue your request for a connection and receive a Future<Connection>back.Better idle connection handling. Instead of closing connections directly, it can still pool connections and sizes the idle pool with a smarter algorithm.You can decide at what moment connections are considered abandoned, is it when the pool is full, or directly at a timeout
          by specifying a pool usage threshold.
      The abandon connection timer will reset upon a statement/query activity. Allowing a connections that is in use for a long time to not timeout.
          This is achieved using the ResetAbandonedTimerClose connections after they have been connected for a certain time. Age based close upon return to the pool.
      Get JMX notifications and log entries when connections are suspected for being abandoned. This is similar to
          the removeAbandonedTimeoutbut it doesn't take any action, only reports the information.
          This is achieved using thesuspectTimeoutattribute.Connections can be retrieved from a java.sql.Driver,javax.sql.DataSourceorjavax.sql.XADataSourceThis is achieved using thedataSourceanddataSourceJNDIattributes.XA connection support | 
 | How to use |  | 
  
    Usage of the Tomcat connection pool has been made to be as simple as possible, for those of you that are familiar with commons-dbcp, the
    transition will be very simple. Moving from other connection pools is also fairly straight forward.
   | Additional features |  | 
    The Tomcat connection pool offers a few additional features over what most other pools let you do: 
      initSQL- the ability to run a SQL statement exactly once, when the connection is createdvalidationInterval- in addition to running validations on connections, avoid running them too frequently.jdbcInterceptors- flexible and pluggable interceptors to create any customizations around the pool,
          the query execution and the result set handling. More on this in the advanced section.fairQueue- Set the fair flag to true to achieve thread fairness or to use asynchronous connection retrieval | 
 | Standalone |  | 
    
      The connection pool only has another dependency, and that is on tomcat-juli.jar.
      To configure the pool in a stand alone project using bean instantiation, the bean to instantiate is
      org.apache.tomcat.jdbc.pool.DataSource. The same attributes (documented below) as you use to configure a connection
      pool as a JNDI resource, are used to configure a data source as a bean. | 
 | JMX |  | 
    
      The connection pool object exposes an MBean that can be registered.
      In order for the connection pool object to create the MBean, the flag jmxEnabledhas to be set to true.
      This doesn't imply that the pool will be registered with an MBean server, merely that the MBean is created.
      In a container like Tomcat, Tomcat itself registers the DataSource with the MBean server, theorg.apache.tomcat.jdbc.pool.DataSourceobject will then register the actual
      connection pool MBean.
      If you're running outside of a container, you can register the DataSource yourself under any object name you specify,
      and it propagates the registration to the underlying pool. To do this you would callmBeanServer.registerMBean(dataSource.getPool().getJmxPool(),objectname).
      Prior to this call, ensure that the pool has been created by callingdataSource.createPool(). | 
 | 
 | Attributes |  | 
  To provide a very simple switch to and from commons-dbcp and tomcat-jdbc-pool,
     Most attributes are the same and have the same meaning. | JNDI Factory and Type |  | 
    | Attribute | Description | 
|---|
 | factory | factory is required, and the value should be org.apache.tomcat.jdbc.pool.DataSourceFactory |  | type | Type should always be javax.sql.DataSourceorjavax.sql.XADataSource Depending on the type a org.apache.tomcat.jdbc.pool.DataSourceor aorg.apache.tomcat.jdbc.pool.XADataSourcewill be created. | 
 | 
 | Common Attributes |  | 
  These attributes are shared between commons-dbcp and tomcat-jdbc-pool, in some cases default values are different. | Attribute | Description | 
|---|
 | defaultAutoCommit | (boolean) The default auto-commit state of connections created by this pool. If not set, default is JDBC driver default (If not set then the setAutoCommitmethod will not be called.) |  | defaultReadOnly | (boolean) The default read-only state of connections created by this pool. If not set then the setReadOnlymethod will not be called. (Some drivers don't support read only mode, ex: Informix) |  | defaultTransactionIsolation | (String) The default TransactionIsolation state of connections created by this pool. One of the following: (see javadoc ) 
           NONEREAD_COMMITTEDREAD_UNCOMMITTEDREPEATABLE_READSERIALIZABLE If not set, the method will not be called and it defaults to the JDBC driver. |  | defaultCatalog | (String) The default catalog of connections created by this pool. |  | driverClassName | (String) The fully qualified Java class name of the JDBC driver to be used. The driver has to be accessible
         from the same classloader as tomcat-jdbc.jar
       |  | username | (String) The connection username to be passed to our JDBC driver to establish a connection.
         Note that method DataSource.getConnection(username,password)by default will not use credentials passed into the method,
         but will use the ones configured here. SeealternateUsernameAllowedproperty for more details. |  | password | (String) The connection password to be passed to our JDBC driver to establish a connection.
         Note that method DataSource.getConnection(username,password)by default will not use credentials passed into the method,
         but will use the ones configured here. SeealternateUsernameAllowedproperty for more details. |  | maxActive | (int) The maximum number of active connections that can be allocated from this pool at the same time.
         The default value is 100 |  | maxIdle | (int) The maximum number of connections that should be kept in the pool at all times.
         Default value is  maxActive:100Idle connections are checked periodically (if enabled) and
         connections that been idle for longer thanminEvictableIdleTimeMilliswill be released. (also seetestWhileIdle) |  | minIdle | 
        (int) The minimum number of established connections that should be kept in the pool at all times.
        The connection pool can shrink below this number if validation queries fail.
        Default value is derived from initialSize:10(also seetestWhileIdle) |  | initialSize | (int)The initial number of connections that are created when the pool is started.
         Default value is 10 |  | maxWait | (int) The maximum number of milliseconds that the pool will wait (when there are no available connections)
         for a connection to be returned before throwing an exception.
         Default value is 30000(30 seconds) |  | testOnBorrow | (boolean) The indication of whether objects will be validated before being borrowed from the pool.
         If the object fails to validate, it will be dropped from the pool, and we will attempt to borrow another.
         In order to have a more efficient validation, see validationInterval.
         Default value isfalse |  | testOnConnect | (boolean) The indication of whether objects will be validated when a connection is first created.
         If an object fails to validate, it will be throw SQLException.
         Default value isfalse |  | testOnReturn | (boolean) The indication of whether objects will be validated before being returned to the pool.
         The default value is false. |  | testWhileIdle | (boolean) The indication of whether objects will be validated by the idle object evictor (if any).
         If an object fails to validate, it will be dropped from the pool.
         The default value is falseand this property has to be set in order for the
         pool cleaner/test thread is to run (also seetimeBetweenEvictionRunsMillis) |  | validationQuery | (String) The SQL query that will be used to validate connections from this pool before returning them to the caller.
         If specified, this query does not have to return any data, it just can't throw a SQLException.
         The default value isnull.
         If not specified, connections will be validation by the isValid() method.
         Example values areSELECT 1(mysql),select 1 from dual(oracle),SELECT 1(MS Sql Server) |  | validationQueryTimeout | (int) The timeout in seconds before a connection validation queries fail.  This works by calling 
         java.sql.Statement.setQueryTimeout(seconds)on the statement that executes thevalidationQuery.
         The pool itself doesn't timeout the query, it is still up to the JDBC driver to enforce query timeouts. 
         A value less than or equal to zero will disable this feature. 
         The default value is-1. |  | validatorClassName | (String) The name of a class which implements the
         org.apache.tomcat.jdbc.pool.Validatorinterface and
         provides a no-arg constructor (may be implicit). If specified, the
         class will be used to create a Validator instance which is then used
         instead of any validation query to validate connections. The default
         value isnull. An example value iscom.mycompany.project.SimpleValidator. |  | timeBetweenEvictionRunsMillis | (int) The number of milliseconds to sleep between runs of the idle connection validation/cleaner thread.
         This value should not be set under 1 second. It dictates how often we check for idle, abandoned connections, and how often
         we validate idle connections.
         The default value is 5000(5 seconds).
 |  | numTestsPerEvictionRun | (int) Property not used in tomcat-jdbc-pool. |  | minEvictableIdleTimeMillis | (int) The minimum amount of time an object may sit idle in the pool before it is eligible for eviction.
         The default value is 60000(60 seconds). |  | accessToUnderlyingConnectionAllowed | (boolean) Property not used. Access can be achieved by calling unwrapon the pooled connection.
         seejavax.sql.DataSourceinterface, or callgetConnectionthrough reflection or
         cast the object asjavax.sql.PooledConnection |  | removeAbandoned | (boolean) Flag to remove abandoned connections if they exceed the removeAbandonedTimeout.
         If set to true a connection is considered abandoned and eligible for removal if it has been in use
         longer than theremoveAbandonedTimeoutSetting this totruecan recover db connections from
         applications that fail to close a connection. See alsologAbandonedThe default value isfalse. |  | removeAbandonedTimeout | (int) Timeout in seconds before an abandoned(in use) connection can be removed.
         The default value is 60(60 seconds). The value should be set to the longest running query your applications
         might have. |  | logAbandoned | (boolean) Flag to log stack traces for application code which abandoned a Connection.
         Logging of abandoned Connections adds overhead for every Connection borrow because a stack trace has to be generated.
         The default value is false. |  | connectionProperties | (String) The connection properties that will be sent to our JDBC driver when establishing new connections.
         Format of the string must be [propertyName=property;]*
         NOTE - The "user" and "password" properties will be passed explicitly, so they do not need to be included here.
         The default value is null. |  | poolPreparedStatements | (boolean) Property not used. |  | maxOpenPreparedStatements | (int) Property not used. | 
 | 
 | Tomcat JDBC Enhanced Attributes |  | 
  | Attribute | Description | 
|---|
 | initSQL | (String) A custom query to be run when a connection is first created.
         The default value is null. |  | jdbcInterceptors | (String) A semicolon separated list of classnames extending
         org.apache.tomcat.jdbc.pool.JdbcInterceptorclass.
         See Configuring JDBC interceptors
         below for more detailed description of syntax and examples. 
         These interceptors will be inserted as an interceptor into the chain
         of operations on a java.sql.Connectionobject.
         The default value isnull. 
         Predefined interceptors:
 org.apache.tomcat.jdbc.pool.interceptor.- keeps track of auto commit, read only, catalog and transaction isolation level.ConnectionState
 org.apache.tomcat.jdbc.pool.interceptor.- keeps track of opened statements, and closes them when the connection is returned to the pool.StatementFinalizer
 
         More predefined interceptors are described in detail in the
         JDBC Interceptors section.
       |  | validationInterval | (long) avoid excess validation, only run validation at most at this frequency - time in milliseconds.
         If a connection is due for validation, but has been validated previously within this interval, it will not be validated again.
         The default value is 3000(3 seconds). |  | jmxEnabled | (boolean) Register the pool with JMX or not.
         The default value is true. |  | fairQueue | (boolean) Set to true if you wish that calls to getConnection should be treated
         fairly in a true FIFO fashion. This uses the org.apache.tomcat.jdbc.pool.FairBlockingQueueimplementation for the list of the idle connections. The default value istrue.
         This flag is required when you want to use asynchronous connection retrieval.Setting this flag ensures that threads receive connections in the order they arrive.
 During performance tests, there is a very large difference in how locks
         and lock waiting is implemented. When
 fairQueue=truethere is a decision making process based on what operating system the system is running.
         If the system is running on Linux (propertyos.name=Linux.
         To disable this Linux specific behavior and still use the fair queue, simply add the propertyorg.apache.tomcat.jdbc.pool.FairBlockingQueue.ignoreOS=trueto your system properties
         before the connection pool classes are loaded. |  | abandonWhenPercentageFull | (int) Connections that have been abandoned (timed out) wont get closed and reported up unless
         the number of connections in use are above the percentage defined by abandonWhenPercentageFull.
         The value should be between 0-100.
         The default value is0, which implies that connections are eligible for closure as soon
         asremoveAbandonedTimeouthas been reached. |  | maxAge | (long) Time in milliseconds to keep this connection. When a connection is returned to the pool,
         the pool will check to see if the now - time-when-connected > maxAgehas been reached,
         and if so, it closes the connection rather than returning it to the pool.
         The default value is0, which implies that connections will be left open and no age check
         will be done upon returning the connection to the pool. |  | useEquals | (boolean) Set to true if you wish the ProxyConnectionclass to useString.equalsand set tofalsewhen you wish to use==when comparing method names. This property does not apply to added interceptors as those are configured individually.
         The default value istrue. |  | suspectTimeout | (int) Timeout value in seconds. Default value is 0.Similar to to the
 removeAbandonedTimeoutvalue but instead of treating the connection
           as abandoned, and potentially closing the connection, this simply logs the warning iflogAbandonedis set to true. If this value is equal or less than 0, no suspect
           checking will be performed. Suspect checking only takes place if the timeout value is larger than 0 and
           the connection was not abandoned or if abandon check is disabled. If a connection is suspect a WARN message gets
           logged and a JMX notification gets sent once. |  | rollbackOnReturn | (boolean) If autoCommit==falsethen the pool can terminate the transaction by calling rollback on the connection as it is returned to the pool
          Default value isfalse.
 |  | commitOnReturn | (boolean) If autoCommit==falsethen the pool can complete the transaction by calling commit on the connection as it is returned to the pool
          IfrollbackOnReturn==truethen this attribute is ignored.
          Default value isfalse.
 |  | alternateUsernameAllowed | (boolean) By default, the jdbc-pool will ignore the
         DataSource.getConnection(username,password)call, and simply return a previously pooled connection under the globally configured propertiesusernameandpassword, for performance reasons. 
         The pool can however be configured to allow use of different credentials
         each time a connection is requested.  To enable the functionality described in the
         DataSource.getConnection(username,password)call, simply set the propertyalternateUsernameAllowedtotrue.Should you request a connection with the credentials user1/password1 and the connection
         was previously connected using different user2/password2, the connection will be closed,
         and reopened with the requested credentials. This way, the pool size is still managed
         on a global level, and not on a per schema level.
 The default value is
 false.This property was added as an enhancement to bug 50025.
 |  | dataSource | (javax.sql.DataSource) Inject a data source to the connection pool, and the pool will use the data source to retrieve connections instead of establishing them using the java.sql.Driverinterface.
         This is useful when you wish to pool XA connections or connections established using a data source instead of a connection string. Default value isnull |  | dataSourceJNDI | (String) The JNDI name for a data source to be looked up in JNDI and then used to establish connections to the database. See the dataSourceattribute. Default value isnull |  | useDisposableConnectionFacade | (boolean) Set this to true if you wish to put a facade on your connection so that it cannot be reused after it has been closed. This prevents a thread holding on to a
                   reference of a connection it has already called closed on, to execute queries on it. Default value is true. |  | logValidationErrors | (boolean) Set this to true to log errors during the validation phase to the log file. If set to true, errors will be logged as SEVERE. Default value is falsefor backwards compatibility. |  | propagateInterruptState | (boolean) Set this to true to propagate the interrupt state for a thread that has been interrupted (not clearing the interrupt state). Default value is falsefor backwards compatibility. |  | ignoreExceptionOnPreLoad | (boolean) Flag whether ignore error of connection creation while initializing the pool.
         Set to true if you want to ignore error of connection creation while initializing the pool.
         Set to false if you want to fail the initialization of the pool by throwing exception.
         The default value is false. |  | useStatementFacade | (boolean) Set this to true if you wish to wrap statements in order to
         enable equals()andhashCode()methods to be
         called on the closed statements if any statement proxy is set.
         Default value istrue. | 
 | 
 | 
 | Advanced usage |  | 
  | JDBC interceptors |  | 
    To see an example of how to use an interceptor, take a look at
    org.apache.tomcat.jdbc.pool.interceptor.ConnectionState.
    This simple interceptor is a cache of three attributes, transaction isolation level, auto commit and read only state,
    in order for the system to avoid not needed roundtrips to the database. Further interceptors will be added to the core of the pool as the need arises. Contributions are always welcome! Interceptors are of course not limited to just java.sql.Connectionbut can be used to wrap any
    of the results from a method invocation as well. You could build query performance analyzer that provides JMX notifications when a
    query is running longer than the expected time. | 
 | Configuring JDBC interceptors |  | 
    Configuring JDBC interceptors is done using the jdbcInterceptors property.
    The property contains a list of semicolon separated class names. If the
    classname is not fully qualified it will be prefixed with the
    org.apache.tomcat.jdbc.pool.interceptor.prefix. Example:
 
      jdbcInterceptors="org.apache.tomcat.jdbc.pool.interceptor.ConnectionState;
        org.apache.tomcat.jdbc.pool.interceptor.StatementFinalizer"
      is the same as
 
  jdbcInterceptors="ConnectionState;StatementFinalizer" 
    Interceptors can have properties as well. Properties for an interceptor
    are specified within parentheses after the class name. Several properties
    are separated by commas.
     Example:
 
      jdbcInterceptors="ConnectionState;StatementFinalizer(useEquals=true)"
     
    Extra whitespace characters around class names, property names and values
    are ignored.
     | 
 | org.apache.tomcat.jdbc.pool.JdbcInterceptor |  | 
    Abstract base class for all interceptors, can not be instantiated. | Attribute | Description | 
|---|
 | useEquals | (boolean) Set to true if you wish the ProxyConnectionclass to useString.equalsand set tofalsewhen you wish to use==when comparing method names.
         The default value istrue. | 
 | 
 | org.apache.tomcat.jdbc.pool.interceptor.ConnectionState |  | 
    Caches the connection for the following attributes autoCommit,readOnly,transactionIsolationandcatalog.
       It is a performance enhancement to avoid roundtrip to the database when getters are called or setters are called with an already set value. | 
 | org.apache.tomcat.jdbc.pool.interceptor.StatementCache |  | 
    Caches PreparedStatementand/orCallableStatementinstances on a connection. The statements are cached per connection.
       The count limit is counted globally for all connections that belong to
       the same pool. Once the count reaches max, subsequent
       statements are not returned to the cache and are closed immediately. | Attribute | Description | 
|---|
 | prepared | (boolean as String) Enable caching of PreparedStatementinstances created usingprepareStatementcalls.
           The default value istrue. |  | callable | (boolean as String) Enable caching of CallableStatementinstances created usingprepareCallcalls.
           The default value isfalse. |  | max | (int as String) Limit on the count of cached statements across
           the connection pool.
           The default value is 50. | 
 | 
 | org.apache.tomcat.jdbc.pool.interceptor.QueryTimeoutInterceptor |  | 
    Automatically calls java.sql.Statement.setQueryTimeout(seconds)when a new statement is created.
       The pool itself doesn't timeout the query, it is still up to the JDBC driver to enforce query timeouts. | Attribute | Description | 
|---|
 | queryTimeout | (int as String) The number of seconds to set for the query timeout.
           A value less than or equal to zero will disable this feature.
           The default value is 1seconds. | 
 | 
 | org.apache.tomcat.jdbc.pool.interceptor.SlowQueryReport |  | 
    Keeps track of query performance and issues log entries when queries exceed a time threshold of fail.
       The log level used is WARN | Attribute | Description | 
|---|
 | threshold | (int as String) The number of milliseconds a query has to exceed before issuing a log alert.
           The default value is 1000milliseconds. |  | maxQueries | (int as String) The maximum number of queries to keep track of in order to preserve memory space.
           A value less than or equal to 0 will disable this feature.
           The default value is 1000. | 
 | 
 | org.apache.tomcat.jdbc.pool.interceptor.SlowQueryReportJmx |  | 
    Extends the SlowQueryReportand in addition to log entries it issues JMX notification
       for monitoring tools to react to. Inherits all the attributes from its parent class.
       This class uses Tomcat's JMX engine so it wont work outside of the Tomcat container.
       By default, JMX notifications are sent through the ConnectionPool mbean if it is enabled.
       TheSlowQueryReportJmxcan also register an MBean ifnotifyPool=false | Attribute | Description | 
|---|
 | notifyPool | (boolean as String) Set to false if you want JMX notifications to go to the SlowQueryReportJmxMBean
           The default value istrue. |  | objectName | (String) Define a valid javax.management.ObjectNamestring that will be used to register this object with the platform mbean server
           The default value isnulland the object will be registered using
           tomcat.jdbc:type=org.apache.tomcat.jdbc.pool.interceptor.SlowQueryReportJmx,name=the-name-of-the-pool | 
 | 
 | org.apache.tomcat.jdbc.pool.interceptor.ResetAbandonedTimer |  | 
    
        The abandoned timer starts when a connection is checked out from the pool.
        This means if you have a 30second timeout and run 10x10second queries using the connection
        it will be marked abandoned and potentially reclaimed depending on the abandonWhenPercentageFullattribute.
        Using this interceptor it will reset the checkout timer every time you perform an operation on the connection or execute a
        query successfully. | 
 | 
 | Code Example |  | 
  Other examples of Tomcat configuration for JDBC usage can be found in the Tomcat documentation.  | Plain Ol' Java |  | 
    Here is a simple example of how to create and use a data source.   import java.sql.Connection;
  import java.sql.ResultSet;
  import java.sql.Statement;
  import org.apache.tomcat.jdbc.pool.DataSource;
  import org.apache.tomcat.jdbc.pool.PoolProperties;
  public class SimplePOJOExample {
      public static void main(String[] args) throws Exception {
          PoolProperties p = new PoolProperties();
          p.setUrl("jdbc:mysql://localhost:3306/mysql");
          p.setDriverClassName("com.mysql.jdbc.Driver");
          p.setUsername("root");
          p.setPassword("password");
          p.setJmxEnabled(true);
          p.setTestWhileIdle(false);
          p.setTestOnBorrow(true);
          p.setValidationQuery("SELECT 1");
          p.setTestOnReturn(false);
          p.setValidationInterval(30000);
          p.setTimeBetweenEvictionRunsMillis(30000);
          p.setMaxActive(100);
          p.setInitialSize(10);
          p.setMaxWait(10000);
          p.setRemoveAbandonedTimeout(60);
          p.setMinEvictableIdleTimeMillis(30000);
          p.setMinIdle(10);
          p.setLogAbandoned(true);
          p.setRemoveAbandoned(true);
          p.setJdbcInterceptors(
            "org.apache.tomcat.jdbc.pool.interceptor.ConnectionState;"+
            "org.apache.tomcat.jdbc.pool.interceptor.StatementFinalizer");
          DataSource datasource = new DataSource();
          datasource.setPoolProperties(p);
          Connection con = null;
          try {
            con = datasource.getConnection();
            Statement st = con.createStatement();
            ResultSet rs = st.executeQuery("select * from user");
            int cnt = 1;
            while (rs.next()) {
                System.out.println((cnt++)+". Host:" +rs.getString("Host")+
                  " User:"+rs.getString("User")+" Password:"+rs.getString("Password"));
            }
            rs.close();
            st.close();
          } finally {
            if (con!=null) try {con.close();}catch (Exception ignore) {}
          }
      }
  }
 | 
 | As a Resource |  | 
    And here is an example on how to configure a resource for JNDI lookups <Resource name="jdbc/TestDB"
          auth="Container"
          type="javax.sql.DataSource"
          factory="org.apache.tomcat.jdbc.pool.DataSourceFactory"
          testWhileIdle="true"
          testOnBorrow="true"
          testOnReturn="false"
          validationQuery="SELECT 1"
          validationInterval="30000"
          timeBetweenEvictionRunsMillis="30000"
          maxActive="100"
          minIdle="10"
          maxWait="10000"
          initialSize="10"
          removeAbandonedTimeout="60"
          removeAbandoned="true"
          logAbandoned="true"
          minEvictableIdleTimeMillis="30000"
          jmxEnabled="true"
          jdbcInterceptors="org.apache.tomcat.jdbc.pool.interceptor.ConnectionState;
            org.apache.tomcat.jdbc.pool.interceptor.StatementFinalizer"
          username="root"
          password="password"
          driverClassName="com.mysql.jdbc.Driver"
          url="jdbc:mysql://localhost:3306/mysql"/>
 | 
 | Asynchronous Connection Retrieval |  | 
     The Tomcat JDBC connection pool supports asynchronous connection retrieval without adding additional threads to the
        pool library. It does this by adding a method to the data source called Future<Connection> getConnectionAsync().
        In order to use the async retrieval, two conditions must be met: 
          An example of using the async feature is show below.You must configure the fairQueueproperty to betrue.You will have to cast the data source to org.apache.tomcat.jdbc.pool.DataSource   Connection con = null;
  try {
    Future<Connection> future = datasource.getConnectionAsync();
    while (!future.isDone()) {
      System.out.println("Connection is not yet available. Do some background work");
      try {
        Thread.sleep(100); //simulate work
      }catch (InterruptedException x) {
        Thread.currentThread().interrupt();
      }
    }
    con = future.get(); //should return instantly
    Statement st = con.createStatement();
    ResultSet rs = st.executeQuery("select * from user");
 | 
 | Interceptors |  | 
    Interceptors are a powerful way to enable, disable or modify functionality on a specific connection or its sub components.
       There are many different use cases for when interceptors are useful. By default, and for performance reasons, the connection pool is stateless.
       The only state the pool itself inserts are defaultAutoCommit,defaultReadOnly,defaultTransactionIsolation,defaultCatalogif
       these are set. These 4 properties are only set upon connection creation. Should these properties be modified during the usage of the connection,
       the pool itself will not reset them. An interceptor has to extend the org.apache.tomcat.jdbc.pool.JdbcInterceptorclass. This class is fairly simple,
       You will need to have a no arg constructor   public JdbcInterceptor() {
  }
       When a connection is borrowed from the pool, the interceptor can initialize or in some other way react to the event by implementing the
       public abstract void reset(ConnectionPool parent, PooledConnection con);
       method. This method gets called with two parameters, a reference to the connection pool itself ConnectionPool parentand a reference to the underlying connectionPooledConnection con. 
       When a method on the java.sql.Connectionobject is invoked, it will cause the   public Object invoke(Object proxy, Method method, Object[] args) throws Throwable
       method to get invoked. The Method methodis the actual method invoked, andObject[] argsare the arguments.
       To look at a very simple example, where we demonstrate how to make the invocation tojava.sql.Connection.close()a noop
       if the connection has been closed   if (CLOSE_VAL==method.getName()) {
      if (isClosed()) return null; //noop for already closed.
  }
  return super.invoke(proxy,method,args);
        There is an observation being made. It is the comparison of the method name. One way to do this would be to do
        "close".equals(method.getName()).
        Above we see a direct reference comparison between the method name andstatic final Stringreference.
        According to the JVM spec, method names and static final String end up in a shared constant pool, so the reference comparison should work.
        One could of course do this as well:   if (compare(CLOSE_VAL,method)) {
      if (isClosed()) return null; //noop for already closed.
  }
  return super.invoke(proxy,method,args);
        The compare(String,Method)will use theuseEqualsflag on an interceptor and do either reference comparison or
        a string value comparison when theuseEquals=trueflag is set. Pool start/stopWhen the connection pool is started or closed, you can be notifed. You will only be notified once per interceptor class
       even though it is an instance method. and you will be notified using an interceptor currently not attached to a pool.
   public void poolStarted(ConnectionPool pool) {
  }
  public void poolClosed(ConnectionPool pool) {
  }
       When overriding these methods, don't forget to call super if you are extending a class other than JdbcInterceptor Configuring interceptorsInterceptors are configured using the
 jdbcInterceptorsproperty or thesetJdbcInterceptorsmethod.
       An interceptor can have properties, and would be configured like this   String jdbcInterceptors=
    "org.apache.tomcat.jdbc.pool.interceptor.ConnectionState(useEquals=true,fast=yes)"
Interceptor propertiesSince interceptors can have properties, you need to be able to read the values of these properties within your
       interceptor. Taking an example like the one above, you can override the
 setPropertiesmethod.   public void setProperties(Map<String, InterceptorProperty> properties) {
     super.setProperties(properties);
     final String myprop = "myprop";
     InterceptorProperty p1 = properties.get(myprop);
     if (p1!=null) {
         setMyprop(Long.parseLong(p1.getValue()));
     }
  }
 | 
 | Getting the actual JDBC connection |  | 
    Connection pools create wrappers around the actual connection in order to properly pool them.
       We also create interceptors in these wrappers to be able to perform certain functions.
       If there is a need to retrieve the actual connection, one can do so using the javax.sql.PooledConnectioninterface.   Connection con = datasource.getConnection();
  Connection actual = ((javax.sql.PooledConnection)con).getConnection();
 | 
 | 
 | Building |  | 
  We build the JDBC pool code with 1.6, but it is backwards compatible down to 1.5 for runtime environment. For unit test, we use 1.6 and higher Other examples of Tomcat configuration for JDBC usage can be found in the Tomcat documentation.  | Building from source |  | 
    Building is pretty simple. The pool has a dependency on tomcat-juli.jarand in case you want theSlowQueryReportJmx   javac -classpath tomcat-juli.jar \
        -d . \
        org/apache/tomcat/jdbc/pool/*.java \
        org/apache/tomcat/jdbc/pool/interceptor/*.java \
        org/apache/tomcat/jdbc/pool/jmx/*.java
       A build file can be found in the Tomcat source repository.
     
      As a convenience, a build file is also included where a simple build command will generate all files needed.
       ant download  (downloads dependencies)
  ant build     (compiles and generates .jar files)
  ant dist      (creates a release package)
  ant test      (runs tests, expects a test database to be setup)
      The system is structured for a Maven build, but does generate release artifacts. Just the library itself.
     | 
 | 
 |