The Apache Tomcat Servlet/JSP Container

Apache Tomcat 7

Version 7.0.81, Aug 11 2017
Apache Logo

Links

Contents

Installation

Installation

In order to use Tomcat for developing web applications, you must first install it (and the software it depends on). The required steps are outlined in the following subsections.

JDK

Tomcat 7.0 was designed to run on Java SE 6.

Compatible JDKs for many platforms (or links to where they can be found) are available at http://www.oracle.com/technetwork/java/javase/downloads/index.html.

Tomcat

Binary downloads of the Tomcat server are available from http://tomcat.apache.org/. This manual assumes you are using the most recent release of Tomcat 7. Detailed instructions for downloading and installing Tomcat are available here.

In the remainder of this manual, example shell scripts assume that you have set an environment variable CATALINA_HOME that contains the pathname to the directory in which Tomcat has been installed. Optionally, if Tomcat has been configured for multiple instances, each instance will have its own CATALINA_BASE configured.

Ant

Binary downloads of the Ant build tool are available from http://ant.apache.org/. This manual assumes you are using Ant 1.8 or later. The instructions may also be compatible with other versions, but this has not been tested.

Download and install Ant. Then, add the bin directory of the Ant distribution to your PATH environment variable, following the standard practices for your operating system platform. Once you have done this, you will be able to execute the ant shell command directly.

CVS

Besides the required tools described above, you are strongly encouraged to download and install a source code control system, such as the Concurrent Version System (CVS), to maintain historical versions of the source files that make up your web application. Besides the server, you will also need appropriate client tools to check out source code files, and check in modified versions.

Detailed instructions for installing and using source code control applications is beyond the scope of this manual. However, CVS server and client tools for many platforms (along with documentation) can be downloaded from http://www.cvshome.org/.

Comments

Notice: This comments section collects your suggestions on improving documentation for Apache Tomcat.

If you have trouble and need help, read Find Help page and ask your question on the tomcat-users mailing list. Do not ask such questions here. This is not a Q&A section.

The Apache Comments System is explained here. Comments may be removed by our moderators if they are either implemented or considered invalid/off-topic.


Copyright © 1999-2017, Apache Software Foundation